Object Creation - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Objects can be created offline in the system database on the BCT and later downloaded to the host device as part of the edited database. You can also create objects online with a browser if you have the Access Privileges to configure objects using the Security Administrator System. The user interface screens and procedures are similar in either case. Creating an object involves placing it at the desired position in the Navigation Tree and defining all the attributes that are required for it to operate. The procedure begins with the Insert Menu, and a wizard guides you through all the necessary configuration steps.

See the Creating Items with Wizards section for the steps to create objects/items.