Values/Options/Range - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Based on the attribute’s data type, this column may show the range of valid values or a reference to the set of possible values for this attribute. If the complete set of values for the attribute is small, all possible values are shown in this column.