BACnet Notes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The BACnet Notes column specifies if the attribute is exposed as a standard BACnet property and if it can be modified from a BACnet network. The types listed in Table 1 may also appear in the Note column, as applicable.

Table 1. BACnet [System] Notes

Note

Definition

B - Exposed as Standard BACnet Property

Indicates that the attribute can be accessed as a standard BACnet Property of the equivalent BACnet Object Type from a BACnet network.

W - Writable

Indicates that the value of the attribute can be modified by a message from a device on the BACnet network.