Updates the Present Value at Command Priority Operator Override (8).
The Operator Override command sends the specified command to the internal supervisory device object, which is then only sent to the field device when one of the following conditions is met: a) NOT Local Control and NOT Out Of Service, or b) NOT Local Control and after issuing the In Service command.
Back to Multistate Value Commands.