Reflects the current value of the multistate value object as one of n states, where n is the number of states defined in the Number of States attribute. The Present Value is equal to the last value corresponding to the States Text attribute. Present Value is optionally commandable. If Present Value is commandable for a given object instance, then Priority Array and Relinquish Default are also present for that instance. If Out of Service is true, Present Value is writable.
Back to Multistate Value Attributes.