Multistate Value Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.

Table 1. Multistate Value Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

BACnet Notes1

Initial Value

Values/Options/Range

Number of States

Number

CW 2

W

4

2–32

Out of Service

True or False

   

False

Always False

Present Value 3

One value from a set

DRW

DRW

 

States Text attribute identifies the value set for this attribute.

Priority Array 4

Set of values

       

Reliability 5

One value from a set

W

W

Reliable

No Fault Detected (Reliable), Multistate Fault, Unreliable Other

Uses Reliability (Set 503).

State Text

Set of values

       

States Text

One value from a set

CW

CW

   

Status Flags

Series of True or False states

     

In Alarm, Fault, Overridden, Out of Service

Uses BAC Status Flags (Set 9).

1 C - Configurable, D - Default Attribute for Display, R - Affected by Object’s Reliability, W - Writable
2 Not writable through the MS/TP integration. Must be configured through CCT.
3 If Present Value is commandable, then it must be writable. If Out of Service is True, this attribute is True.
4 If Present Value is commandable, both these attributes are present.
5 The Reliability attribute is always present in supervisory device implementations.