Heavy Equipment Delay - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Indicates the amount of time that this output point adds to the Accumulated Delay attribute of the Heavy Equipment Controller object when this point is started. The next output point is delayed by that amount of time of the HEC Accumulated Delay is not already decremented to zero.

The supervisory device’s five internal Heavy Equipment Controller objects (see HED Controller) time their delays independently of one another. For example, HED 1 and HED 4 can count down their delays at the same time.

Back to Multistate Output Attributes.