HED Controller - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The supervisory device has five internal Heavy Equipment Controller objects for use by Binary Output and Multistate Output objects. The BO and MO objects reference the HED controller objects by number (1–5).

All BO and MO objects on a supervisory device share the five internal HED controller objects. For example, if BO1 and MO3 on Device-1 reference HED controller 1, they are using the same HED controller.

Also see Heavy Equipment Delay.

Back to Multistate Output Attributes.