Multistate Output Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.
Table 1. Multistate Output Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

BACnet Notes1

Initial Value

Values/Options/Range

Device Type

Text

CW

W

 

Limit: 20 characters

Heavy Equipment Delay

Number

CW

Not supported

0

Range: 0–255 Seconds

HED Controller

Number

CW

Not supported

 

1–5

Number of States

Number

CW

W

4

2–16

Out of Service

True or False

CW

W

 

False

True

Present Value

One value from a set

DRW

DRW

 

States Text attribute identifies the value set for this attribute.

Priority Array

Set of values

       

Reliability

One value from a set

   

Reliable

No Fault Detected (Reliable), Open Loop, Shorted Loop, No Output, Unreliable Other

Uses Reliability (Set 503).

State Text

One state from a set

   

Off Low

Med Hi

 

States Text

One state from a set

CW

CW

Off Low

Med Hi

 

Status Flags

One value from a set

     

In Alarm, Fault, Overridden, Out of Service

Uses BAC Status Flags (Set 9).

1 C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Object’s Reliability, W - Writable