Multistate Input Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.

Table 1. Multistate Input Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

BACnet Notes1

Initial Value

Values/Options/Range

Device Type

Text

CW

W

Null

Limit: 20 characters

Number of States

Number

CW

W

4

Minimum Value = 2

Maximum Value = 16

Out of Service

True or False

CW

W

False

False

True

Present Value 2

One value from a set

DNRW

DNRW

 

States Text attribute identifies the value set for this attribute.

Reliability

One value from a set

W

W

 

No Fault Detected (Reliable), No Sensor, Over Range, Under Range, Open Loop, Shorted Loop, Multi State Fault, Unreliable Other Uses Reliability (Set 503).

State Text

Set of Values

       

States Text

One value from a set

CW

C

Off Low

Med Hi

 

Status Flags

Series of True or False states

     

In Alarm, Fault, Overridden, Out of Service Uses BAC Status Flags (Set 9).

1 C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Object’s Reliability, W - Writable
2 This attribute is required to be writable if Out of Service is True.