Enable - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Specifies that (when the Multiple Command object is enabled) the object it is capable of issuing commands.

Back to Multiple Command Commands.