Send OK - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Indicates the success or failure of the subordinate commands. If any subordinate commands failed, this attribute is set to False. When a send error is detected, a 5-minute timer is set. When the timer expires, the object is reevaluated and all commands are sent again. Commands may fail if the subordinate object is off-box and offline or if the subordinate object is set for local control.

Back to Multiple Command Attributes.