Relinquish Default - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Specifies the default value to be used for the Present Value attribute when no commands are currently controlling this object. If this attribute is configured to any value other than None, the object sends commands for the value immediately.

Back to Multiple Command Attributes.