Multiple Command Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.
Table 1. Multiple Command Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

Initial Value

Values/Options/Range

Enabled

True or False

     

Executing

True or False

 

False

False, True

Execution Priority

One state from a set

CW

   

Last Executed Date

Date

N

   

Last Executed Time

Time

N

   

Number of States

Number

C

4

1–32

Present Value

One state from a set

DW

 

States Text attribute identifies the states set for this attribute.

Send OK

True or False

     

States Text

One state from a set

C

States

 
Table 2. Multiple Command Object Attributes - Action Tables Tab

Attribute Name

Data Type

Notes 2

Initial Value

Values/Options/Range

Action Table (State0. . . StateN)

List of Command References

CW

 
Object Reference, Delay, Command ID, Parameters, Priority
Note: The total number of commands identified in the Action Table 1 command set should not exceed 40.

Command Priority

One state from a set

CW

16

Uses Write Priority (Set 1).

Number of States

Number

C

4

1–32

Relinquish Default

One state from a set

CNW

   

States Text

One state from a set

C

States

 
1 C - Configurable, D - Default Attribute for Display, N - Value Not Required, W - Writable
2 C - Configurable, D - Default Attribute for Display, N - Value Not Required, W - Writable