Multiple Command Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

The Multiple Command object issues a series of commands to multiple objects by means of a single command action. Commanding this object results in the execution of the commands for the given state. This object supports States 1–32.

This object allows a user to start building controls for the day with one command or to prevent selected points from generating COS and alarm messages when a control point is in a specified state (Auto Shutdown).

For example, based on a single input, such as Room Occupied, a defined set of actions can occur: setpoint goes to 72˚, a fan comes on, lights come on, and the door unlocks.

For general information on BCPro system objects, see the Common Object Attributes section.

For more information on the wizard used to create Multiple Command objects, see the Insert Object - Multiple Command section.