Extended Labels - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Menu Selection: View > Extended Labels (select the check box)

Toggles the display of the item labels in the All Items navigation tree or user navigation tree from standard to extended. An extended label shows the BACnet object name that was defined when the object was initially created in braces next to the standard label. This is the name used in the object's Fully Qualified Reference. The BCPro object name may be the same as the BACnet object name, or it may have been edited as a label that is more recognizable to the user.

Example:

Standard Label = Field Bus1

Extended Label = Field Bus1{Field Bus1}