Create Backup - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Menu Selection: Tools > Database > Create Backup

Creates a backup file for the active archive database. If needed, the archive database can be restored using the Tools > Database > Restore Backup menu option. See the Restore Archive Wizard.

The backup file is always named <archive>.backup, where <archive> is the name of the open archive visible at the top of the BCT navigation tree. Do not rename the backup file (renaming a backup file causes a subsequent restore to fail). To save different versions, copy the backup file to different subdirectories.

The default path is

C:\ProgramData\Johnson Controls\BCMIII\DatabaseFiles