Rename - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Menu Selection: Action > Rename

Renames the selected supervisory device in the BCT.
Note: When renaming a BCPro Workstation, the name must match the host name of the computer on which the Workstation is installed.
Note: This rename option may take a while to complete because it changes the database references to the device.