Import Integration - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Menu Selection: Action > Import Integration

This command is only available when an Integration under a device is selected in the All Items tree. After adding an Integration, you can select the integration in the navigation tree and use this menu selection to add existing devices and points under the integration.