MS/TP Field Bus Integration Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.
Table 1. MS/TP Field Bus Integration Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

Initial Value

Values/Options/Range

APDU Retries

Number

CW

3

0–65,535

APDU Timeout

Number

CW

12,000

0–65,535

Milliseconds

APDU Segment Timeout

Number

CW

11,000

0–65,535

Milliseconds

Baud Rate Selection

One state/type/ mode from a set

CW

0

Uses MSTPDL Baud Rate (Set 300).

See the attribute description.

Count

Number

     

Device Discovery Range

List

CW

 

Network number, high limit device instance, low limit device instance

Discover All As General BACnet Device

True or False

CW

False

 

Execution Priority

One set from a state

CW

Normal

 

Internode Comm Timer

Number

CW

120

Range = 5–255

Max APDU Length

Number

CW

480

Legal values are:

50

128

206

480

Max Master

Number

CW

127

4–127

Page Size

Number

CW

1,000

10–65,535

Periodic Update

Number

CW

20

0–65,535

Units = seconds

Poll Delay

Number

CW

0

10–50

Units = milliseconds

Preserve Discovered Devices

True or False

CW

True

 

Requested Vendor ID

Number

CN

 

The current list of Vendor IDs can be viewed at http://www.bacnet.org/VendorID/BACnet%20Vendor%20IDs.htm

Synchronize Time

True or False

CW

False

 

Synchronize Time Zone

True or False

CW

False

 
Table 2. MS/TP Field Bus Integration Attributes - Diagnostic Tab

Attribute Name

Data Type

Notes2

Initial Value

Values/Options/Range

Active Baud Rate

One state/type/ mode from a set

   

Uses MSTPDL Baud Rate (Set 300).

See the attribute description.

Broadcast Receive Rate

Number

   

Units = Per Minute

Broadcast Receives

Number

   

0–4,294,967,295

Broadcast Transmits

Number

   

Units = Per Minute

Broadcast Transmit Rate

Number

   

0–4,294,967,295

Buffer Overflows

Number

   

0–4,294,967,295

Bus Analysis Date

Date

     

Bus Analysis Time

Time

     

Bus Analysis Progress

One state/type/ mode from a set

   

See the MS/TP Analysis Set.

Bus Device Configuration List

List

     

Bus Health Index

Number

     

Bus Performance Index

Number

     

Bytes In

Number

   

0–4,294,967,295

Bytes Out

Number

   

0–4,294,967,295

Data CRC Errors

Number

   

0–4,294,967,295

Data Expecting Reply Frames Rxed

Number

   

0–4,294,967,295

Data Expecting Reply Frames Txed

Number

   

0 - 4,294,967,295

Data Not Expecting Reply Frames Rxed

Number

   

0–4,294,967,295

Data Not Expecting Reply Frames Txed

Number

   

0–4,294,967,295

Duplicate Device Identifiers

List

     

Execution Time

Number

 

0

0–4,294,967,295

Units = seconds

Framing Errors

Number

   

0–4,294,967,295

Header CRC Errors

Number

   

0–4,294,967,295

Internal Errors

Number

   

0–4,294,967,295

Lost Token

Number

   

0–4,294,967,295

Max Output Queue Used

Number

   

1–65,534

Maximum Token Loop Time

Number

   

0–4,294,967,295

Milliseconds

Overrun Errors

Number

   

0–4,294,967,295

PFM Frames Rxed

Number

   

0–4,294,967,295

PFM Frames Txed

Number

   

0–4,294,967,295

Packets Timed Out

Number

   

0–4,294,967,295

Packets Too Long

Number

   

0–4,294,967,295

Polled Object Count

Number

     

Port Status

One state/type/

mode from a set

   

Uses MSTPDL Port Status (Set 302).

Predicted Token Loop Time

Number

   

Milliseconds

Reply Postponed Frames Rxed

Number

   

0–4,294,967,295

Reply Postponed Frames Txed

Number

   

0–4,294,967,295

Reply Too Slow Application Errors

Number

   

0–4,294,967,295

Reply Too Slow Datalink Errors

Number

   

0–4,294,967,295

Reset Date

Date

     

Reset Time

Time

     

Retries

Number

   

0–4,294,967,295

Test Request Frames Rxed

Number

   

0–4,294,967,295

Test Request Frames Txed

Number

   

0–4,294,967,295

Token Frames Rxed

Number

   

0–4,294,967,295

Token Frames Txed

Number

   

0–4,294,967,295

Token Loop Time

Number

   

0–4,294,967,295

Milliseconds

Unexpected Frames Rxed

Number

   

0–4,294,967,295

Weighted Bus Health Constant

Number

W

0.5

Minimum = 0.10

Maximum: 0.99

Weighted Bus Performance Constant

Number

W

0.5

Minimum = 0.10

Maximum: 0.99

1 C - Configurable, W - Writable, N - Value Not Required
2 C - Configurable, W - Writable, N - Value Not Required