Interlock Configuration - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Configure the attributes of the Focus/Configuration, Interlock Definition, and Action Tables tabs of the Interlock object. See the Interlock Attributes section for descriptions of the attributes on these tabs.

On the Focus/Configuration tab, click the Advanced radio button to view and edit all the attributes available on this tab.

On the Interlock Definition tab, define the items/objects to control and the desired conditional logic. Tips for this tab include:
  • Click the Add button to add items to the list from the Select Item dialog box.
  • Click the check box next to an item in the list and click Delete to remove the item from the list.
  • Select the type of logic to use for the items in the list from the Logic menu. See the Logic attribute description for the types of logic.
On the Action Tables tab, define the commands and the priority for the items/objects under control. Tips for this tab include:
  • Check the All Commands Priority check box if you wish to use the same priority for all commands in the action tables. Clear the All Commands Priority check box to enable individual priority selection for the commands in the action tables.
  • For the Actions for Condition: True and Actions for Condition: False tables, click the Add button to add items to the table from the Select Item dialog box.
  • For the Actions for Condition: True and Actions for Condition: False sections, click the check box next to an item in the table and click Delete if you want to remove the item from the table.