Operator Override - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Updates the Present Value at Command Priority Operator Override.

Important: The Operator Override command sends the specified command to the internal NxE object, which is then only sent to the field device when one of the following conditions is met: a) NOT Local Control and NOT Out Of Service, or b) NOT Local Control and after issuing the In Service command.

Back to Interlock Commands.