Source - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Lists objects whose attributes are used for input into the logic expression to decide if the condition is True or False. Information needed:
  • Item - Name of the source object
  • Attribute - Varies according to object. Default = Present Value
  • Relation - Equal, Not Equal, Greater Than, Less Than, Greater Than or Equal, Less Than or Equal
  • Value - The value used in the Relation. Varies according to the object.
  • Differential - Accounts for variations in the value. Required (and only used) if the value is analog.

Back to Interlock Attributes.