Restore Command Priority - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Selects which commands (at a selected priority) persist through a device restart. When the bit is set, the command (at a selected priority) is saved at shutdown and restored at startup.

Back to Interlock Attributes.