Executing - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Specifies the current execution status of the object. It is True when the object receives a state command and starts sending commands. When all actions are completed for a given state, this flag is set to False.

Back to Interlock Attributes.