Interlock Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.
Table 1. Interlock Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

Initial Value

Values/Options/Range

Executing

True or False

 

False

 

Execution Priority

One state from a set

CW

   

Last Executed Date

Date

N

   

Last Executed Time

Time

N

   

Present Value

One state from a set

DRW

   

Priority Array

Set of values

     

Reliability

One state from a set

   

Uses Reliability (Set 503).

Restore Command Priority

Series of True or False states

CW

Operator Override

 

Send OK

True or False

     

States Text

One state from a set

CW

 

States Text defaults to False/True, but you can use any two state set.

Table 2. Interlock Object Attributes - Interlock Definition Tab

Attribute Name

Data Type

Notes 2

Initial Value

Values/Options/Range

Logic

One state from a set

CW

0

Match All (AND)

Match Any (OR)

Complex

Logic Equations

Text

CW

 

Maximum 56 characters

Source

List of value sets

CW

 

Item/Object Name

Attribute

Relation (Equal, Not Equal, Greater Than, Less Than, Greater Or Equal, Less Or Equal)

Value

Differential (required and only used when the value is analog)

Table 3. Interlock Object Attributes - Action Tables Tab

Attribute Name

Data Type

Notes 3

Initial Value

Values/Options/Range

Action Tbl 1 (True)

List of Command References

CW

 

Item/Object Name

Command

Priority

Delay (0–65,535 seconds)

Parameters (vary according to command)

Action Tbl 2 (False)

List of Command References

CW

 

Item/Object Name

Command

Priority

Delay (0–65,535 seconds)

Parameters (vary according to command)

Commands Priority

One state from a set

CW

16

Uses Write Priority (Set 1).

1 C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Object Reliability, W - Writable
2 C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Object Reliability, W - Writable
3 C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Object Reliability, W - Writable