Priority for Writing - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Defines the priority at which the referenced attributes are commanded. Seven is the highest priority and 16 is the lowest supported by the Global Data Sharing object, with the default of 15.

Note: We do not recommend using priorities 7 or 8 as they may interfere with the operator override function.