Global Data Sharing Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Global Data Sharing object provides a means for distributing information about changes in a single attribute value to other attribute reference points. This minimizes hardware costs and system complexity. For example, a Router or Gateway might have multiple AHUs on its network, but only one has an outdoor air sensor. The Global Data Sharing object can share the value from the single sensor with the other AHUs.

The data types defined for the Global Data Sharing object’s input and corresponding outputs should match. Otherwise, each output attempts to convert the value being received to the data type defined for it. The software does not check for data type consistency. Global data sharing is restricted to within one site.

For general information on BCPro system objects, see Common Object Attributes.