Memory Usage - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

It is calculated as follows:

(Total commit charge / Commit charge limit) x 100

These values are obtained from the WindowsOS. Memory usage can be used to diagnose operational problems with the device. For example, if the value climbs steadily over time (about 24 hours), it would indicate a memory leak. A memory leak eventually consumes all system RAM and causes a device reset. Valid data is provided only on the Gateway hardware. Under device simulation, the value is 0.

If your computer’s hard disk is formatted to use FAT32 (32-bit File Allocation Table), the simulated value for the Memory Usage attribute is not accurate.

Back to Gateway Attributes.