Specifies the current battery charging state in a Modbus Gateway. A value of False indicates the battery contains at least 80% of full charge capacity and is not currently recharging. A value of True indicates the battery contains less than 80% of full charge capacity and is currently charging.
If the Battery Charging value is True and the battery is charging, the battery stops charging when it is 100% charged. Trend this attribute value to determine the current battery charge cycle time. In Simulation, this attribute is False.
Back to Gateway Attributes.