Gateway Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab and the Diagnostics tab.

Click the attribute name in the table for a description of the attribute.

Table 1. Workstation Device Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Flags 1

Initial Value

Values/Options/Range 2

APDU Retries 2

Number

CW

4

2–10

APDU Segment Timeout 2

Number

CW

10,000

1,000–65,535

Units = milliseconds

APDU Timeout 2

Number

CW

10,000

1,000–65,535

Units = milliseconds

Archive Date

Date

     
BIOS Version

Text

     
Firmware Version

Text

     
Local Date

Date

     
Local Time

Time

     
Model Name

Text

 

CN-BIG1970-0

 
Power Consecutive Samples

Number

CW

5

0–32

Power Sampling Interval

Number

CW

1

0–32

Units = Seconds

Version

Number

     
Table 2. Workstation Device Object Attributes - Diagnostic Tab

Attribute Name

Data Type

Flags 3

Initial Value

Values/Options/Range 4

Battery Charging

True or False

   

This attribute appears in only the BACnet Router and Modbus Gateway.

Battery Condition

One from a list of conditions

   

Uses Ok Fault (Set 161) or Battery Condition (Set 175).

Board Temperature

Real value

   

Units = Deg C

Display Precision = 1

COV Increment = 1.0

CPU Usage

Real value

   

Units = %

Memory Usage

Number

   

Units = %

Display Precision = 0.01

COV Increment = 0.1

Table 3. Gateway Device Object Attributes - Network Tab

Attribute Name

Data Type

Flags 5

Initial Value

Values/Options/Range 6

Computer Name 7

Text

W

 

See attribute description.

DHCP Enabled

True or False

CW

True (1)

0 = DHCP disabled

1 = DHCP enabled

DNS Server IP Addresses

List of numbers

CW

 

List of IP addresses.

Domain Name 7

Text

W

   
Ethernet MAC Address

List of numbers

     
IP Address

List of numbers

CW

 

Any valid IP address

IP Mask

List of numbers

CW

   
IP Router Address

List of numbers

CW

   
Obtain DNS Address Automatically

True or False

CW

True (1)

 
1 C - Configurable, N - Value Not Required, Q - BACnet Required, W - Writable
2 If you write the value of this attribute, you must restart the Gateway for the new settings to take effect.
3 C - Configurable, N - Value Not Required, Q - BACnet Required, W - Writable
4 If you write the value of this attribute, you must restart the Gateway for the new settings to take effect.
5 C - Configurable, N - Value Not Required, Q - BACnet Required, W - Writable
6 If you write the value of this attribute, you must reset the Gateway for the new settings to take effect.
7 If you change the value of this attribute, the Gateway automatically resets.