Gateway Device Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Gateway object defines the attributes that represent the externally visible characteristics of the BCPro Gateway. One Gateway Device object exists per BCPro Gateway.

Note: The Object Type for this object is labeled Device in the software.

This object allows you to see data about the controller, such as the IP address and the current date and time.

For general information on BCPro system objects, see the Object Help section.