Folder - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

A Folder object helps support the hierarchical organization of objects.

A total of 1000 objects can be added per folder, and up to 10 consecutive levels of Folder objects can be added within any other folder or object.

Note: You must name a new folder differently from the folders in the default set on the user interface.

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section.