Total Record Count - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Represents the total number of records collected by the Trend Extension since creation. When the value of Total Record Count reaches its maximum possible value of 0XFFFFFFFF, the next value it takes is zero. Once this value has wrapped to zero, its semantic value (the total number of records collected) is lost, but its use in generating notifications remains.

Back to Trend Extension Attributes.