Specifies the time and date to disable logging. If the Stop Time contains any wildcard values, then the conditions to disable logging based on time are ignored. Logging is disable if the Stop Time is prior to the Start Time. When the Trend object is inactive due to the current time being outside of the Start Time or Stop Time, the Status attribute reflects this state (assuming it is the highest priority status). A change in the active/inactive state due to the Start Time/Stop Time value has no impact on the Enable attribute. If the Trend object was disabled due to the Stop Time, the Trend object attempts to send the trend samples to the server. If you define a Stop Time that is before the Start Time, the Trend object is disabled.
Back to Trend Extension Attributes.