Start Time - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Specifies the time and date to enable logging when the Enable attribute is set to True. If the Start Time contains any wildcard values, then the conditions to enable logging based on time are ignored. When the Trend object is inactive due to the current time being outside of the Start Time or Stop Time, the Status attribute reflects this state (assuming it is the highest priority status). If you define a Stop Time that is before the Start Time, the Trend object is disabled.

Back to Trend Extension Attributes.