Sample Interval - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Specifies the periodic time in seconds for which the referenced property is logged. If this attribute is zero, samples are recorded using COV reporting.

Note: If you want to takes samples on a COV, set the value of this attribute to 0 seconds.
Note: Otherwise, configure the Sample Interval at 60 seconds or higher to prevent loss of trend data and reduction in performance of the BCPro Workstation, Router, and Gateway devices that receive samples from the configured trend.

Back to Trend Extension Attributes.