Enables transferring of the trend sample data to the BCPro Workstation when this attribute is set to True and the buffer fills to the level specified by the Transfer Setpoint attribute.
Note: If you create multiple trend extensions on a single point and send it to an Historical Data Repository, then setting Repository Enabled to true will cause the Trend Viewer and/or Trend Study to display a combination of 15 minute and 1 minute samples. If Repository enabled is set to False then the Trend viewer displays only the data from the selected Trend Extension. To use multiple trends on a single object in an Historical Data Repository, create duplicate AV or BV objects that map to the point in question, then create a new trend on the parallel AV or BV.
Back to Trend Extension Attributes.