Indicates the sequence number associated with the most recently collected record whose collection triggered a notification (that is, it caused the value of the Record Since Notify attribute to be equal to or greater than the value of the Notify Threshold attribute). If no notification has occurred since logging began, the value of this attribute is 0.
Back to Trend Extension Attributes.