Event Enable - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Determines whether notifications are enabled for To Fault and To Normal events. A To Normal transition occurs when the value of the Record Since Notify attribute is equal to or greater than the value of the Notify Threshold attribute. A To Fault transition occurs when an attempted COV subscription fails. The To Normal transition must be enabled and set by default. The Read and write methods ensure that this value cannot be set to False.

Back to Trend Extension Attributes.