Deleting Extensions - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

About this task

Note: You cannot delete an extension in online mode with Basic Access.

Procedure

  1. To delete extensions (using the Navigation Tree):
    1. Select the item from the navigation tree and select Show Extensions from the Action menu.
    2. Select the check box of the extension that you want to delete.
    3. Click Delete.
  2. To delete extensions (when the item is in the Display Frame):
    1. View the extension.
    2. Select the tab for the extension.
    3. Select the extension.
    4. Click Delete.