Creating Extensions - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

About this task

Note: You cannot create an extension in online mode with Basic Access.

To create extensions:

Procedure

  1. Select the item from the Navigation Tree and select Show Extensions from the Action Menu.
    Note: Alternatively, you can create extensions when prompted upon completion of a wizard, or when the item is in the Display Frame by selecting the tab for the extension and clicking new.
  2. Select New for the type of extension that you want to create. The corresponding Extension Wizard appears.
  3. Click Browse to select the attribute that you want to associate with the item.
  4. Complete the information on the wizard screens. The screens vary depending on the type of extension you arecreating. See the Wizards section for help on using wizards.
  5. Select Finish on the summary page to create the extension.