APDU Segment Timeout - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Indicates the amount of time in milliseconds between retransmission of an APDU segment. This value is non-zero if the device supports segmentation of transmitted APDUs.

Back to Ethernet IP Datalink Attributes.