APDU Retries - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Indicates the maximum number of times that an APDU is retransmitted. If the device does not perform retries, it is set to zero. If this value is greater than zero, a non-zero value appears in the APDU Timeout attribute.

Back to Ethernet IP Datalink Attributes.