Ethernet IP Datalink Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.

Table 1. Ethernet IP Datalink Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

Initial Value

Values/Options/Range

Address Length

Number

     

APDU Retries

Number

CW

4

2-10

APDU Segment Timeout

Number

CW

10,000

1,000–65,535

Units = milliseconds

APDU Timeout

Number

CW

10,000

1,000–65,535

Units = milliseconds

BACnet IP Port

Number

 

47,808

 

Broadcast Address

Text

   

Maximum length = 6 octets

Device Address

Text

   

Maximum length = 6 octets

Max APDU Length

Number

CW

1,024

128–65,535

Units = bytes

Network Address

Number

     
Table 2. Ethernet IP Datalink Attributes - Diagnostic Tab

Attribute Name

Data Type

Notes 2

Initial Value

Values/Options/Range

Broadcast Receives

Number

     

Broadcast Transmit

Number

     

Discarded Frames

Number

     

Message Recieves

Number

     

Message Transmits

Number

     

Reset Date

Date

     

Reset Time

Time

     

Retry Attempts

Number

     

Transmit Failures

Number

     
1 C - Configurable, W - Writable
2 C - Configurable, W - Writable