Ethernet IP Datalink Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Ethernet IP Datalink object manages the Ethernet communications bus and the messages transmitted on it. Working with this object allows you to access Ethernet card statistics.

For general information on BCPro system objects, see the Object Help section.