Upload - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

The Manage Archive Wizard Upload option transfers a copy of the BCPro Workstation, Router, or Gateway archive database into the archive database of the BCT. Perform an upload to update the BCT archive database with changes made in the online mode. The BCPro Workstation, Router, or Gateway database overwrites the BCT archive database for the device being loaded. The direction of an upload is from the BCPro Workstation, Router, or Gateway to the BCT. Figure 1 and Table 1 describe the upload process.

Note: To ensure recent online changes are captured during an upload, manually archive the device (Actions > Commands > Archive) and then upload. The archive function moves data from the Router or Gateway RAM to its nonvolatile memory, from which it then can be uploaded. Do not confuse the archive function within the device with the archive database that is in BCT.
Figure 1. Upload Process

Table 1. Upload Process

Number

Process Description

1

After configuring an upload in the Manage Archive Wizard, the Manage Archive Wizard sends the upload command to the ActionQ feature in the BCT.

2

The ActionQ locks the BCPro Workstation, Router, or Gateway in the archive database. See Database Locking.

3

  1. The ActionQ begins the upload process at the time defined for uploading the BCPro Workstation, Router, or Gateway database.
  2. The BCPro Workstation, Router, or Gateway creates an archive file of its database.

4

  1. The ActionQ transfers the BCPro Workstation, Router, or Gateway archive file to the BCT archive database.
  2. The ActionQ replaces the existing archive database with the BCPro Workstation, Router, or Gateway archive file.

5

  1. The ActionQ unlocks the BCPro Workstation, Router, or Gateway in the archive database.
  2. The ActionQ displays the final status of the upload.