Upgrading Device - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English
The Manage Archive Wizard upgrade device option upgrades the version of a Router or Gateway within the Archive database. If the BCPro Workstation is not already upgraded, include it to allow upgrades to the current BCT Version. You may schedule the load for later by selecting the Schedule upgrade radio button and entering a date and time.
Table 1. Upgrade Device Process

Number

Process Description

1

After configuring an upgrade device in the Manage Archive Wizard, the Manage Archive Wizard sends the upload command to the ActionQ feature in the BCT.

2

The ActionQ locks the BCPro Workstation, Router, or Gateway in the archive database. See Database Locking.

3

  1. The ActionQ begins the upload process at the time scheduled in the upgrading device wizard.
  2. The Router or Gateway within the Archive database is upgraded. If the BCPro Workstation is upgraded, it also allows upgrades to the current BCT Version.

4

The ActionQ displays the final status of the upgrade device.