The Manage Archive Wizard Download option transfers a copy of the BCT archive database into the BCPro Workstation, Router, or Gateway database. Perform a download to send the changes made in the SCT database to the BCPro Workstation, Router, or Gateway database. The BCT archive database overwrites the BCPro Workstation, Router, or Gateway database. The direction of a download is from the BCT to the device or BCPro Workstation. At the end of the download, the BCPro Workstation, Router, or Gateway restarts and does not control or monitor the system until the restart is complete. The following figure and table describe the download process.
|
Number |
Process Description |
|---|---|
|
1 |
After configuring a download in the Manage Archive Wizard, the Manage Archive Wizard sends the download command to the ActionQ in the BCT. |
|
2 |
|
|
3 |
The ActionQ transfers the BCT archive database file to the BCPro Workstation, Router, or Gateway database. |
|
4 |
|