Database Locking - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

After scheduling a load, the archive database for that device is locked in the BCT until all loads for that device have completed or are deleted. Only the device being loaded is locked. You can still access devices that have no scheduled loads.

If you need to edit the archive database in the BCT for a device with a scheduled load (locked device), you can still delete the load to clear the lock. After making your changes, you can schedule the load again.